Issue
The EM4800 communications are intermittent despite being able to continuously ping the device
Product Line
EM4800
Environment
Power Monitoring Expert 8.1
Cause
The communications are slower on the network that the device is on than anticipated
Resolution
Go to devices in Management console.
Right click on the device and click properties.
Right click in the white space and select advanced properties.
Change the Receive Timeout from 10,000 to 20,000.
The EM4800 communications are intermittent despite being able to continuously ping the device
Product Line
EM4800
Environment
Power Monitoring Expert 8.1
Cause
The communications are slower on the network that the device is on than anticipated
Resolution
Go to devices in Management console.
Right click on the device and click properties.
Right click in the white space and select advanced properties.
Change the Receive Timeout from 10,000 to 20,000.
Released for:Schneider Electric Global