How many EtheNet/IP adapters can be managed by LMC078?
There is no fix maximum of EtheNet/IP adapters managed by LMC078 as EtherNet/IP scanner (there is limit 16 on M251). Limit in LMC078 is given by the available load of the CPU, bus cycle task and the amount of transferred data.
Released for:Schneider Electric Global
Explore more
Range:
Modicon LMC058/LMC078
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.