{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to set up an ATV320 with terminals as run command and 0-10VDC reference from AI1?
Issue:
Trying to set an ATV320 with terminals as run command and 0-10VDC reference from AI1.

Product Line:
Altivar 320

Environment:
All

Cause:
Programing

Resolution:
Wiring:
DI1 and +24V as 2 wire control run command.

0-10VDC can be wired into AI1 and COM.
If using a potentiometer then wiring would look like +10, AI1, and COM.

Drive is already programmed to do this function from the factory.
Under CONF, FULL, I/O, TCC will need to be set to 2C.
Under CONF, FULL, CTL, FR1 will need to be set to AI1

Schneider Electric Global