{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why does SoMove show no DTM installed on the Home screen?

Issue:
No DTM files in SoMove.

Product Line:
SoMove Software and DTM Library Install

Environment:
MS Windows


Resolution:
In SoMove, on the upper right corner, click on "List the device software installed on this PC" under "Installed Device Information"
A window will open showing Installed DTMs
If you have downloaded and installed DTMs for specific products, and see no installed DTMs,

click the [Update Catalog] button.
If that doesn't resolve the issue;

- Exit SoMove Software
- Uninstall manually any installed DTM (from: Control Panel/Programs..)
- If any SoMove or SoMove Launcher instance running - Have to End it from Windows Task Manager/Processes
- Now reinstall ATVxx DTM, Right Click and select Run as Administrator
- Launch SoMove --> When prompted, click Update Catalogue --> DTM(s) will now appear in that list, and be available under

[Create a Project Offline]


Below are links for SoMove Software and DTMs for AC Drives and Softstarts.

(Somove: latest version)
https://www.se.com/us/en/download/document/SoMove_FDT/

(Altivar DTM files for the ATV61, ATV71, ATV12, ATV212, ATV312, ATV32)
https://www.se.com/ww/en/download/document/Altivar_DTM_Library/
(Altivar Process 600 DTM files)
https://www.se.com/ww/en/download/document/ATV6xx_DTM_Library_EN/

(Altivar Process 900 DTM files)
https://www.se.com/us/en/download/document/ATV9xx_DTM_Library_EN/

(Altistart DTM files for ATS22 and ATS48)
https://www.se.com/ww/en/download/document/Altistart_DTM_Library/

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.