Issue
What recommendations are available for Printing from Unity Pro
Product Line
Unity,
Environment
Windows 10
Resolution
If printing is a known requirement for Unity Pro Project Logic, then here are some tips that may help.
-
Plan for the need to print and...
-
Choose a page size for printing before creating any logic
-
Test the printing of all Unity Pro Languages to determine the settings required to achieve optimized desired results
-
Use a single and common Number of Columns for all LD Sections in the Project
-
Use the Unity Pro Project Settings to fix the Column Size of LD Sections
-
Comments can be added to rows to serve as page break guides
-
-
Create FBD Section logic with regards to the page size and page breaks
-
Comments can be added to FBD Sections to serve as page break guides
-
it is recommended to use the Standard FBD Column and Row settings
-
-
The Number of Columns in SFC Sections must be managed to the test determined limit by the user
-
-
Keep in mind the following...
-
Unity Pro only prints the occupied Columns and Rows used in FBD, LD and SFC Sections
-
Printing to Paper vs. Files has different final result expectations
-
Printing to Paper
-
Achieving acceptable results when printing FBD, LD and SFC Sections will most likely require the use of page sizes larger than 8.5x11
-
-
Printing to Files
-
Optimized results may require a variety of page sizes
-
Searching for Text content is expected
-
-
-
All of this takes time and is most likely not as simple as just clicking Print
-
The Microsoft XPS Document Writer is a recommended printer for printing in Unity Pro. The XPS Document Writer is standard printer installed with Windows.
Here are some testing results from printing to the XPS Document Writer.
FBD Sections
Page Size
Letter
Orientation: Portrait Landscape
Cols-Rows/page: 60x80 90x50
Tabloid
Orientation: Portrait Landscape
Cols-Rows/page: 90x140 150x80
C sheet
Orientation: Portrait Landscape
Cols-Rows/page: 150x180 190x140
D sheet
Orientation: Portrait Landscape
Cols-Rows/page: 190x240 310x180
E sheet
Orientation: Portrait Landscape
Cols-Rows/page: 310x240 360x240
LD Sections
Cells Width: Single Column (1)
Page Size
Letter
Orientation: Portrait Landscape
Cols-Rows/page: 13x27 18x19
Tabloid
Orientation: Portrait Landscape
Cols-Rows/page: 18x47 30x27
C sheet
Orientation: Portrait Landscape
Cols-Rows/page: 30x63 39x47
Cells Width: Double Columns (1)
Page Size
Letter
Orientation: Portrait Landscape
Cols-Rows/page: 6x27 9x19
Tabloid
Orientation: Portrait Landscape
Cols-Rows/page: 9x47 15x27
C sheet
Orientation: Portrait Landscape
Cols-Rows/page: 15x63 19x47
Cells Width: Triple Columns (1)
Page Size
Letter
Orientation: Portrait Landscape
Cols-Rows/page: 4x27 6x19
Tabloid
Orientation: Portrait Landscape
Cols-Rows/page: 6x47 10x27
C sheet
Orientation: Portrait Landscape
Cols-Rows/page: 10x63 13x47
D sheet
Orientation: Portrait Landscape
Cols-Rows/page: 13x100 20x63
Notes:
(1) Setting the Cells Width is in the Project Settings>>Program>>LD
Released for:Schneider Electric Global