Issue:
We are unsure if the EMKA electromechanical release door handle will fit onto a NetShleter SX cabinet.
Product Line:
NetShelter SX
Environment:
All models, all serial numbers.
Cause:
A customer wants to install the EMKA electromechanical release door handle onto a NetShelter SX cabinet.
Resolution:
Yes, the EMKA 1150-U56, 1150-U56-01 and 1150-U58 can be installed onto a NetShelter SX cabinet, but you must reuse the NetShleter SX cam.
We are unsure if the EMKA electromechanical release door handle will fit onto a NetShleter SX cabinet.
Product Line:
NetShelter SX
Environment:
All models, all serial numbers.
Cause:
A customer wants to install the EMKA electromechanical release door handle onto a NetShelter SX cabinet.
Resolution:
Yes, the EMKA 1150-U56, 1150-U56-01 and 1150-U58 can be installed onto a NetShelter SX cabinet, but you must reuse the NetShleter SX cam.
Released for:Schneider Electric Global