Issue:
ATV212 run activate and preset speed on the same input.
Product Line:
S-Flex ATV212
Environment:
All
Cause:
Set up Run and Preset speed at the same time.
Resolution:
Yes. The logic inputs have options for combination assignments.
22 = run forward + preset speed 1
23 = run reverse + preset speed 1
Eg: Logic input F assignment F111 = 22
Input OFF - Motor stops
Input ON - Motor runs forward at speed set by Sr1 (preset speed 1)
ATV212 run activate and preset speed on the same input.
Product Line:
S-Flex ATV212
Environment:
All
Cause:
Set up Run and Preset speed at the same time.
Resolution:
Yes. The logic inputs have options for combination assignments.
22 = run forward + preset speed 1
23 = run reverse + preset speed 1
Eg: Logic input F assignment F111 = 22
Input OFF - Motor stops
Input ON - Motor runs forward at speed set by Sr1 (preset speed 1)
Released for:Schneider Electric Global