Issue:
A customer wants to replace the PDU in a NetShelter CX Mini.
Product Line:
NetShelter CX
Environment:
AR4000MV, all serial numbers.
Cause:
The brochure doesn't show if the PDU is removable.
Resolution:
The PDU that ships installed inside the AR4000MV is removable.
A customer wants to replace the PDU in a NetShelter CX Mini.
Product Line:
NetShelter CX
Environment:
AR4000MV, all serial numbers.
Cause:
The brochure doesn't show if the PDU is removable.
Resolution:
The PDU that ships installed inside the AR4000MV is removable.
Released for:Schneider Electric Global