{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the drive read and display input line current on the ATV61 and ATV71 drives?
Issue:
Can the ATV61/ATV71 read and display supply current or input line current on the default display or in the Drive Menu under 1.2 Monitoring?

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Displaying  input line current.

Resolution:
No you can not read the input line current on the display.  The drive will display motor or load current, however, it is not possible to display supply or line current.