Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

		
Search FAQs
SmartConnect Portal indicates that the firmware is out of date on my SmartConnect enabled UPS. How do I update it?

Article available in these languages: Spanish, Thai


Issue:

SmartConnect Portal indicates that the firmware is out of date on my SmartConnect enabled UPS


Product Line:

Smart-UPS

Environment:

Smart-UPS models with prefix SCL, SMC, SMT, SMTL, SMX, and SRTL, that have an APC SmartConnect Ethernet port that you can use to connect the UPS to Schneider Electric cloud services.


Cause:

SmartConnect enabled Smart-UPS products are able to download the latest UPS Firmware from the Cloud.

Resolution:

1 - To update the firmware you can do so via the cloud portal if you have a valid standard or advanced plan.
See the instructions at the link below
https://community.se.com/t5/Firmware-Upgrade/How-to-Upgrade/ta-p/465745
or view the attached video "SmartConnect Firmware Upgrade".

2 - The other option for updating the firmware is Via the "Configuration" menu on the UPS LCD screen. You can update the UPS firmware by selecting "​Install FW?"
Note: This option will only be seen once a Firmware Image has been automatically downloaded by the UPS from the cloud, and is not available for SCL model Smart-UPS.

Once you select "Install FW?", your options are:
• Next off (Updates the UPS Firmware next time that the UPS is turned off)
• Now (Updates the UPS firmware immediately without interrupting operations)
• Don't Install

The update will take approximately 5 minutes to complete from the time you initiate the update. You may not have a battery backup available during some of this time. If you have a high profile application, you may want to use "Next Off" so that the UPS updates itself the next time you reboot the unit, rather than doing the update live.

3 - Alternatively, update the firmware using the Firmware Upgrade Wizard. See Schneider Electric FA279197: How do I update the firmware of my SRT/SMC/XU/XP/SMX/SMT/SMTL/SCL/SRC/CHS series Smart-UPS using the Firmware Upgrade Wizard?

NOTE: SRTL UPS units with firmware version 5.0 will not receive new UPS firmware via the cloud, and will not notify the user that the UPS firmware is out of date.

Product Line: SRTL2K2RM1UIC, SRTL2K2RM1UC, SRTL3KRM1UIC, SRTL3KRM1UC

The only way to update the firmware of these UPS units is locally using the Smart-UPS Firmware Upgrade Wizard. Refer to FA279197.

This is addressed in UPS firmware version 05.6.

Schneider Electric Global

Attachment(s)
SmartConnect Firmware Upgrade Video.zip [1.66 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Our Mission
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Financial Results
  • Annual Reports
  • Share Price
  • Investor Events
  • Careers
  • Sustainability
  • Electricity 4.0
  • Next-generation Automation
  • AI and Technology
  • Reports
  • Foundation
  • Consulting
  • Global - FR
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Change your cookie settings