Can you retrieve data from the A9MEM3155 modbus meter wireless using a Modbus to WiFi converter?
We recommend using a standard tested SE solution like COM'X with a Wifi dongle, which can be connected to iEM3155 over Modbus RTU and COM'X will send the data of the meter over Wifi.
Released for:Schneider Electric Global
Explore more
Product:
A9MEM3155
Range:
Acti 9 iEM3000
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.