{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
E-FLEX ATV61 drive is running, but not the motor?
Issue:
E-FLEX ATV61 drive is in RUN status with output frequency and voltage, but the motor is not running.

Product Line:
ATV 61
E-Flex

Environment:
All

Cause:
Motor is not running, no motor current

Resolution:

If the E-Flex has the bypass feature, then there will be a TEST/NORMAL switch on the front.  It is possible that the drive may be in TEST mode which would mean that the output circuit to the motor is open.  The VFD Output phase loss feature is inactive, so the drive will be allowed to run.

Schneider Electric Global