Issue:
Planning external uses for the available 24Vdc power supply from the ATV320.
Product line:
ATV320, Altivar 320
Environment:
n/a
Cause:
n/a
Resolution:
The Altivar 320 power supply is rated for 100mA load. Tolerance of the voltage supply is -15% to +20%.
Note that the logic inputs use 7mA each.
Planning external uses for the available 24Vdc power supply from the ATV320.
Product line:
ATV320, Altivar 320
Environment:
n/a
Cause:
n/a
Resolution:
The Altivar 320 power supply is rated for 100mA load. Tolerance of the voltage supply is -15% to +20%.
Note that the logic inputs use 7mA each.
Released for:Schneider Electric Global