{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to change the icon for a Connexium Network Manager Map device.
Issue
How to change the icon ifora Connexium Network Manager Map device.

Product Line
Connexium Network Manager

Environment
Windows 10

Resolution
If Connexium Network Manager does not have a defined icon for the device, the device will be shown as a yellow container box.
sffsr




The following steps can be used to change the icon.
  • Right click on the device icon.
  • Select 'Properties'.
wfr

  • Type in a name for the container
  • Click on the appropriate  button for the icon type (either Realistic or Abstract)
wrr



  • Browse for and select the icon.
  • Click on Open.
eerr


  • Click on OK.
ewr


  • The device will be shown in the network map with the new icon and container name.
rwer



Schneider Electric Global