Issue:
Unable to see nPr in the SIn menu on the Altivar Process ATV630
Product Line:
ATV630
Environment:
All
Cause:
Programming
Resolution:
This occurs when CONF > FULL > DRC- > ASY –
**When the ATV320 replaces ATV312, the correct setting is CoS**
Unable to see nPr in the SIn menu on the Altivar Process ATV630
Product Line:
ATV630
Environment:
All
Cause:
Programming
Resolution:
This occurs when CONF > FULL > DRC- > ASY –
- nPC is set to CoS
**When the ATV320 replaces ATV312, the correct setting is CoS**
Released for:Schneider Electric Global