{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Does the TM241CEC24R have a serial port?
Issue
Does the M241 PLC have a serial port?

Product Line
M241

Resolution
​The TM241CEC24R has two serial ports. The complete M241 line have the two serial ports detailed below.

[Port 1]
RJ45 RS232/RS485.

It can be used to communicate with devices supporting the Modbus protocol as either Client or
Server, ASCII protocol (printer, modem...) and MachineExpert/SoMachine Protocol for HMI.
It also provides  5 Vdc power distribution.

[Port 2]
Terminal block RS-485 only.

It is used to communicate with devices supporting the Modbus protocol as either a
Client or Server and ASCII Protocol (printer, modem...).

Schneider Electric Global