Issue
How many BMXEIA0100 can be used in a M580 architecture?
Product Line
M580, BMXEIA0100
Resolution
16 is the max number of BMXEIA0100 AS-i modules accepted in M580 configuration. This is the global limitation for the M580 system.
With have other limitations on drops & local CPU rack:
=> 2 max on RIO drops with CRA
=> 2 max on level 10 CPU, 4 max on level 20, 6 on level 30 and 8 for above.
How many BMXEIA0100 can be used in a M580 architecture?
Product Line
M580, BMXEIA0100
Resolution
16 is the max number of BMXEIA0100 AS-i modules accepted in M580 configuration. This is the global limitation for the M580 system.
With have other limitations on drops & local CPU rack:
=> 2 max on RIO drops with CRA
=> 2 max on level 10 CPU, 4 max on level 20, 6 on level 30 and 8 for above.
Released for:Schneider Electric Global