{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Which contacts on the Altistart ATS48 or ATS480 can be used to indicate when the motor is running at full speed

The dry contacts used to indicate full speed run status, use R2A/C.  This relay is factory programmed as End Of Start and cannot be changed.  It is a normally open contact that closes when the motor has reached full speed.


If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)