{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do you set up the ATS48 soft starter to read KWs in the SUP menu?
Issue:
Setting up the ATS48 soft starter to read KWs in the SUP menu

Product Line:
ATS48

Environment:
All

Cause:
Wants to read the KW settings in the SUP menu

Resolution:
Since the ATS48 does not measure the power circuit voltage, power is calculated based on the measured amperage and user input voltage.  In the drC menu, set parameter ULn to an average supply voltage. The active power calculated is only as accurate as the ULn setting compared to actual voltage.  The KW power can be viewed in the SUP menu, parameter LAP.