{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What Syslog Server can be used with Unity Pro?
Issue
This resolution indicates the minimum requirements of a Syslog Server to be used with Unity Pro/ Control Expert.

Product Line
EcoStruxure Control Expert (formerly known as Unity Pro)

Environment
Unity Pro v13, BMEP581020 v2.50

Resolution
Unity Pro Syslog is based on RFC 5424 (Transport Mapping for Syslog) and it defines the structure of the message created by the software but some of the available Syslog Server doesn't have the option to use RFC 5424 processing. So these servers will show a message that is not clear for the user as you can see below:
dftghuijk

Schneider Electric recommends to use the WinSyslog as the server or any other Syslog Server that has the features to configure the listener and messages as highlighted in yellow on the pictures below using the RFC 5424 processing.
dfgthyjuiygj

After configure this option on your Syslog server, the messages will show as below and you can see that it is easier to understand the log message.
rdfthyu

Schneider Electric Global