Issue:
Need to find the default IP address for the Link150 (EGX15) Ethernet Gateway
Product Line:
Link150 Ethernet Gateway (EGX150)
Environment:
Link150 Webpage Connection
(EGX150)
Cause:
Unable to connect to the Link150 Ethernet Gateway (EGX150)
Resolution:
The default IP address for the Ethernet Gateway Link150 (EGX150) is 169.254.YY.ZZ
YY.ZZ are the last 2 bytes of the Link150 MAC address. For example, A Link150 with
MAC address 00-B0-D0-86-BB-F7 (hexadecimal) or 0-176-208-134-187-247 (decimal),
set the IP address as169.254.187.247
Need to find the default IP address for the Link150 (EGX15) Ethernet Gateway
Product Line:
Link150 Ethernet Gateway (EGX150)
Environment:
Link150 Webpage Connection
(EGX150)
Cause:
Unable to connect to the Link150 Ethernet Gateway (EGX150)
Resolution:
The default IP address for the Ethernet Gateway Link150 (EGX150) is 169.254.YY.ZZ
YY.ZZ are the last 2 bytes of the Link150 MAC address. For example, A Link150 with
MAC address 00-B0-D0-86-BB-F7 (hexadecimal) or 0-176-208-134-187-247 (decimal),
set the IP address as169.254.187.247
Released for: Schneider Electric Global