Issue:
ATV320 CANopen pinouts for the RJ45 connector.
Product Line:
ATV320 with option card VW3A3608
Environment:
All
Cause:
RJ45 connector pinout on option card VW3A3608.
Resolution:
Pin Layout
Pin 1 = CAN_H
Pin 2 = CAN_L
Pin 3 = CAN_GND
See the attached documents for more programming and CANopen information. Page 31 of NVE41309 12/2017
https://www.se.com/us/en/download/document/NVE41309/
ATV320 CANopen pinouts for the RJ45 connector.
Product Line:
ATV320 with option card VW3A3608
Environment:
All
Cause:
RJ45 connector pinout on option card VW3A3608.
Resolution:
Pin Layout
Pin 1 = CAN_H
Pin 2 = CAN_L
Pin 3 = CAN_GND
See the attached documents for more programming and CANopen information. Page 31 of NVE41309 12/2017
https://www.se.com/us/en/download/document/NVE41309/
Released for:Schneider Electric Global