{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Does M580 Safety CPU support IOscanning?
Yes, it is embedded into the M580 Safety CPUs as it is for other standard M580 CPU using the Distributed I/O Scanner Service that allows non-deterministic communication with distributed Ethernet devices to be integrated into the PlantStruxure™ architecture.

It supports devices using open & standard protocols:
- Modbus/TCP
- EtherNet/IP

Note : M580 safety CPUs can support also safe communication :
- using CIP Safety protocol over EIP
- using specific DFBs and configuration as described in safety manual (REF : QGH46982) to get a safe peer-to-peer communication (safe communication between two M580 CPUs over Modbus/TCP)

Schneider Electric Global