Issue
Configuration of BMXNOM0200 in a EIO to communicate with a serial slave
Product Line
EcoStruxure Control Expert (formerly known as Unity Pro), Modicon M580
Environment
Windows 10 version 1902, Unity Pro v13.1, BMEP585040, BMXNOM0200
Resolution
The BMXNOM0200 can be used on a remote drop (EIO) to read/write data from a modbus serial slave and this video shows the configuration of the ADDMX and READ_VAR function blocks to read a value from a modbus serial slave.
Configuration of BMXNOM0200 in a EIO to communicate with a serial slave
Product Line
EcoStruxure Control Expert (formerly known as Unity Pro), Modicon M580
Environment
Windows 10 version 1902, Unity Pro v13.1, BMEP585040, BMXNOM0200
Resolution
The BMXNOM0200 can be used on a remote drop (EIO) to read/write data from a modbus serial slave and this video shows the configuration of the ADDMX and READ_VAR function blocks to read a value from a modbus serial slave.
Released for:Schneider Electric Global