Does HMIGTO1300/1310 communicate to the Zelio Smart Relay?
Published date:
22 May 2019
Issue:
Does HMIGTO1300/1310 communicate to the Zelio Smart Relay?
Product Line:
HMIGTO1300/HMIGTO1310
Resolution:
No, the HMIGTO1300 / HMIGTO1310 does not communicate to the Zelio Smart Relay. The COM port is a RJ45 connector which only has 8 pins compared to a standard DSUB9 connector which has 9 pins. The missing pin is required for the communication to work with the Zelio Smart Relay.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.