Issue
How many Modbus TCP server paths are supported by a BMENOC0301 and BMENOC0311?
Product Line
BMENOC0301
BMENOC0311
Resolution
With firmware versions 2.08 and higher, BMENOC0301’s and BMENOC0311’s now support a maximum of 64 simultaneous Modbus TCP connections on its server path.
Previous firmware versions supported 32 Modbus TCP connections on its server path.
This information can be found in the BMENOC03x1 Firmware History documentation for firmware version 2.08.
How many Modbus TCP server paths are supported by a BMENOC0301 and BMENOC0311?
Product Line
BMENOC0301
BMENOC0311
Resolution
With firmware versions 2.08 and higher, BMENOC0301’s and BMENOC0311’s now support a maximum of 64 simultaneous Modbus TCP connections on its server path.
Previous firmware versions supported 32 Modbus TCP connections on its server path.
This information can be found in the BMENOC03x1 Firmware History documentation for firmware version 2.08.
Released for:Schneider Electric Global