{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the Harmonized Tariff Schedule (HTS) or US Tariff Code for NetShelter cabinets?
Issue:
A customer needs the HTS for NetShelter SX, SV or VX cabinets.

Product Line:
NetShelter SX, SV, VX

Environment:
All models, all serial numbers.

Cause:
HTS is needed for export.

Resolution:
Harmonized Tariff Schedule and US Tariff code are the same thing.
The HTS for NetShelter SX, SV and VX is 9403.20.0030.

Schneider Electric Global