{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How can we comply the specification requirement of transient over torque is 200%?
As per the catalog specification, if we select the heavy duty drive (ATV630 or ATV930) the maximum transient over current is 150%.

But it is given if you used a motor with one power rating lower. For example, if the drive is a 15kW, to have 150% of over current, the motor used is maximum an 11kW (for standard power rating asynchronous motor). Otherwise, if you need for a 15kW motor, over current of 150% you have to used an 18.5kW drive (Pn+1).
In the case of 200% of over current, the principal is similar. I made an example in the excel file in attachment ("example drive selection.xlsx") and in that case drive have to be taken twice the power of the motor (Pn+2).

Schneider Electric Global

Attachment(s)
example drive selection.xlsx [128.86 KB]