{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the ATV320 be set to maintain running speed if the Modbus communication is lost?

Issue:
Maintain running speed on the ATV320 even if the Modbus communication is lost.

Product Line:
ATV320

Environment:
All

Cause:
Configuration

Resolution:
Yes this can be done.
Parameter SLL in the Com Fault Management menu and can be used to modify the behavior of the VFD after a communication interruption: including the option to run at the last commanded frequency or to run at a fixed (fallback) speed.

Care must be taken to ensure safe operation of the equipment...see the drive programming manual for details.
somove

Schneider Electric Global

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: