The HMI RunTime includes the SiteManager software if the hardware target supports it.
To activate this feature in Vijeo Designer target:
Enter offline mode, click "Main Unit Settings / Remote Viewer Settings", then select "SiteManager Embedded".
To activate this feature in Vijeo Designer target:
Enter offline mode, click "Main Unit Settings / Remote Viewer Settings", then select "SiteManager Embedded".
- In order to start the SiteManager software, set "Remote Management"/"Access Control" to "Enable"
- In order to stop the SiteManager software, set "Remote Management"/"Access Control" to "Disable"
Released for:Schneider Electric Global