{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can plugging and unplugging of Ethernet cables from ports of BMENOC0301 and BMENOC0311 module can generate events which are logged in syslog server.
Yes it is possible to log the following events from BMENOC0301 and BMENOC0311 module to syslog server

1. Ethernet port link status
2. RSTP Topology change
3. FTP Login successful or denied
4. TCP Connection denied due to Access Control List
5. ENOCs Start, Stop, Run

Schneider Electric Global