{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is specfic amount of time that the ATV212 is capable of maintaining running in the event of a momentary power loss?
Issue:
Does the ATV212 have a power loss ride through?

Product line:
ATV212, Altivar 212

Environment:
all

Cause:
Specifications shows the drive can maintain run during a power loss or dip.

Resolution:
The drive can maintain a run in the event of a power loss or dip however too many factors determine for how long of a period this can maintain.  Some of the factors affecting the time are:
Efficiency of each motor pole
The inertia of the load
The size of the drive

The only way to confirm an exact amount of time is to conduct a test on the specific drive and motor installation.