{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why does printing from the HMI stop working after some time?
Issue:
After a period of time, the Magelis HMI will stop outputting to the printer.

Product Line:
Vijeo Designer

Resolution:
It is possible that the HP printer is not configured properly. On the HP printer configuration page, there can be a radio button to append a carriage return to each line feed. Ensure this is enabled to ensure continous printing with your Magelis HMI.