Does RealStream Lift Station use unsolicited messaging in DNP3?
Yes. RealStream has all Alarms (not alerts) setup to do unsolicited messages. This allows the poll rate of the RealStream Lift Station to be set low, but still get real-time alarms from the station.
Released for:Schneider Electric Global
Explore more
Range:
RealStream Lift Station
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.