{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How does the points capacity allocate when routing function is implemented in BMXNOR0200
Question:
How does the points capacity allocate when routing function is implemented in BMXNOR0200?

Answer:
If customer is using routing function(forwarding function), the points counts should include both client side & sever side. So customer have to use half of capacity points(3500) at either client side or sever side.