{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the maximum size of the CoreDB in Easergy T300? What is the maximum number of variables that the T300 can handle?
  • HU250 module includes 1GBit SDRAM memory and each SC150 has 4Mo.
  • The limit of the T300 system comes from the capacity to connect devices (24 SC150 max) upon which the communication could get saturated.
  • However, there are no specific limits concerning the number of variables.

Schneider Electric Global