{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Do NetShelter SX or SV cabinets in NAM have UL stickers? If so, where are they located?
Issue:
A customer needs to know if the NetShelter SX or SV cabinets have UL stickers, and where they are.

Product Line:
NetShelter SX, NetShelter SV.

Environment:
All models, all serial numbers.

Cause:
A customer cannot find the UL sticker location.

Resolution:
NetShelter SX and SV cabinets do ship with a holographic UL sticker.
On the SX cabinet the UL sticker is located on the lower rear frame. Simply open the rear doors and look down.
On the SV cabinet the UL sticker is located on the lower front frame. Simply open the front door and look down.

Schneider Electric Global