{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the recommended wire size and torque for the VW3A3600 module adapter grounding screw?
Issue:
Recommended wire size and torque for the the ATV320 drives VW3A3600 adapter grounding screw.

Product Line:
Altivar ATV320 VW3A3600

Environment:
All

Cause:
Overtorquing the VW3A3600 module ground screw will strip the threads.

Resolution:
The recommended wire size is AWG 14 size wire and the recommended torque is 4.4 lb-in or 0.5 Nm
See the attached instruction bulletin.

Schneider Electric Global

Attachment(s)
VW3A3600 module adapter NVE22661_02.pdf [751.79 KB]