{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video : How to read the data in the Profibus DP Diagnose Service from STBNDP2212 by PRM?
Issue
Profibus slaves has a diagnostic message and STBNDP2212 has 32 bytes with mandatory Profibus DP diagnostic, diagnostic information about the status of the island bus and specific health data

Product Line
Advantys STB, TCSEGPA23F14F (PRM), EcoStruxure Control Expert (formerly known as Unity Pro)

Environment
TCSEGPA23F14F, Unity Pro v13.0, STBNDP2212, Advantys v11

Resolution
The TCSEGPA23F14F (PRM) is a standalone module designed to provide Profibus DPV0 & DPV1 master capability to the M340, M580, Premium and Quantum ranges. This video will show you how to read/interpret the data on Profibus DP diagnose of a STBNDP2212 and you can use it for the module diagnostic. E.g., read the health of each module of the STBNDP2212.