{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
IEC61850 configuration Tool returns the message 'Detected Error in Application'.
Issue
'IEC61850 Configuration Tool' returns 'Detected Error in Application' message.

Product Line
BMENOP0300

Environment
Unity, Windows 10


Resolution
Opening the IEC61850 Configuration Tool returns the message 'Detected Error in Application'.
fggg



The reasons that this occurs could be due to the 'MongoDB' services are not running or they were not properly installed.


To verify that the service are running:
  • Open the 'Computer Management' console.
  • Examine the status of the three (3) Mongo DB services:
  1. MongoDB for SchneiderTools.
  2. MongoDB Infos for SchneiderTools.
  3. MongoDB Transactions for SchneiderTools.
gsgg


If the services are not running:
  • Right click on the service name.
  • Select 'Start '.
  • Retest.



If the services are running:
  • Check that it is not being blocked by either
  1. The firewall,
  2. Antivirus software,
  3. Antispyware software
  4. PC group policy
  • Retest



If the issue still occurs, use the following steps to resolve the issue.
  • Uninstall 'MongoDB 3.2.8 for SchneiderTools'
  1. Open the windows search bar.
  2. Copy the command 'msiexec.exe /x {672788DA-D1E4-41AA-B14D-F0D2044C1180}' and paste it to the Windows Run command text box.
  3. Click on OK.
  4. Click on 'Yes' in the 'Windows Installer' window that appears.
sgs
gsg


  • Reinstall 'MongoDB 3.2.8 for SchneiderTools' using the attached software named 'MongoDB 3.2.8 for SchneiderTools_1.0.9.0_RS_x64.msi.7z.
  • Reinstall the IEC61850 Configuration Tool.
  • Retest.



Schneider Electric Global

Attachment(s)
MongoDB 3.2.8 for SchneiderTools_1.0.9.0_RS_x64.msi.7z [28.29 MB]