Issue:
Wants to wire and program a ATV212 for 3-wire control AND speed reference from the face of the ATV212 drive.
Product Line:
Altivar 212
Environment:
All
Cause:
Setup assistance
Resolution:
1. Wire F terminal for forward Normally Open (NO), momentary close to Start
2. Wire R terminal for Normally Closed (NC) Stop
3. Set Fnod to 3 --speed reference from the face of the drive
4. Set F111 to 2 --forward command on F terminal
5. Set F112 to 49 --3-wire control activated
Wants to wire and program a ATV212 for 3-wire control AND speed reference from the face of the ATV212 drive.
Product Line:
Altivar 212
Environment:
All
Cause:
Setup assistance
Resolution:
1. Wire F terminal for forward Normally Open (NO), momentary close to Start
2. Wire R terminal for Normally Closed (NC) Stop
3. Set Fnod to 3 --speed reference from the face of the drive
4. Set F111 to 2 --forward command on F terminal
5. Set F112 to 49 --3-wire control activated
Released for:Schneider Electric Global