Issue:
Setting up external fault function on ATV212 Drive.
Product Line:
Altivar 212
Environment:
All
Cause:
Configuration for Drive response to External Fault condition.
Resolution:
To set an external fault function, you will need to program one of the logic inputs F/R/or RES as external fault.
Under F--- menu.
F111 is F
F112 is R
F113 is RES terminals.
Let's assume you want to program R as external fault function:
Setting up external fault function on ATV212 Drive.
Product Line:
Altivar 212
Environment:
All
Cause:
Configuration for Drive response to External Fault condition.
Resolution:
To set an external fault function, you will need to program one of the logic inputs F/R/or RES as external fault.
Under F--- menu.
F111 is F
F112 is R
F113 is RES terminals.
Let's assume you want to program R as external fault function:
Set F112 to 11 for external fault where OFF is no detected fault, and ON is where motor stops according to method set by parameter [Ext fault stop mode] (F603).
This will prompt E on display if external fault is on.
F603 options: 0 for freewheel, 1 for ramp stop, 2 for DC braking stop.
This will prompt E on display if external fault is on.
F603 options: 0 for freewheel, 1 for ramp stop, 2 for DC braking stop.
Released for:Schneider Electric Global