{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Where do I find the Coil voltage on the Tesys D 3 Pole AC Contactor?

Article available in these languages: Greek

On the Tesys D 3 Pole AC Contactor you will find the coil voltage marked at the top, behind the Power terminals of the Contactor, for example U7, 240V 50/60 Hz

For the DC Version, the coil voltage is marked on the front of the Contactor. Hence it has got complete part number for the Contactor on the front, for example: LC1D25BD for 24V DC Coil.




Schneider Electric Global

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: