{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the Unity Pro 'Optimized code' check box used for in Project Settings -> General -> Build Settings?
Issue
Definition of the 'Optimized code' option in Project Settings.

Product line
Unity Pro, Control Expert

Resolution
Used to reduce the size of the code generated. Note the following:
  • On Premium PLCs and on Quantum 140 CPU 6•• PLCs, the bit %S18 is no longer managed for arithmetic operations on EDT (Elementary Data Types) and tables.
  • On Quantum 140 CPU 3••/4••/5•• PLCs, the bit %S18 is no longer managed for arithmetic operations on EDT. The bit %S20 is no longer managed for table indexing (the threshold values are still checked).
Modification:
Online possible
Action required:
Build Changes (Offline)
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)