Follow these rules when using tags:
- Place the tag on a solid flat surface or on a window.
- Do not use a tag in an environment with a grill or a mesh: the detection can be very slow or impossible, as the software will have difficulty differentiating between the tag and the grill/mesh.
- Reference photos must be taken directly in front of the tag. The photo plane must be parallel to the tag plane for best results.
- The detection camera plane must be also parallel to the tag plane. If a tag is placed at the top of a scene, consider tilting the tag downward to respect this parallelism. Any deviation from parallel of this photo will reduce the probability of tag detection.
- When identifying the tag placement in the images, use the four corners of the tag itself, as indicated in green here:
Released for:Schneider Electric Global