Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

		
Search FAQs
Com'X 510: Is it possible to simultaneously communicate on RJ-45 or screw terminals, Modbus RS-485 ports?

Issue

Simultaneous Modbus serial communication on RJ45 and removable screw terminal

Product line

Com'X 510 Energy Server

Environment

Meter Communication capability
Modbus Gateway
Modbus Master and Modbus Slave

Resolution

Com'X 510 Energy Server has 1 Modbus RS485 serial port consisting of an RJ45 and removable screw terminal connector (0 V, Screen, D0, D1).

Both connectors are plugged into the same Modbus RS485 serial port and can support 32 devices maximum.

The serial daisy chain or slave devices can be connected to either screw terminals or the RJ45 port, not both at the same time.

Com 'X 510

Refer to FA289876 for documentation for Com'X 510.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Our Mission
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Financial Results
  • Annual Reports
  • Share Price
  • Investor Events
  • Careers
  • Sustainability
  • Electricity 4.0
  • Next-generation Automation
  • AI and Technology
  • Reports
  • Foundation
  • Consulting
  • Global - FR
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Change your cookie settings