{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the stop button on the HMI be disabled as an E-stop when in terminal control mode on an ATV212?
Issue:
ATV212 stop button on the HMI disabling as an E-stop when in terminal control mode

Product Line:
ATV212, SFD212, SFD21

Environment:
All serial numbers

Cause:
Prevent "Flashing E" code. Prevent having to cycle power to clear the drive.

Resolution:
Stop/reset key.
The setting of parameter F734 determines whether it is possible to stop the drive by the Stop key which is located on the drive and graphic display option.
0 = [Enable]    1= [Disable]

Note:
LOSS OF CONTROL
You are going to disable the stop button located on the drive and graphic display option. Do not select 1 unless exterior stopping methods exist.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Schneider Electric Global