undefined undefined
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why can I only use the XBTZ9780 cable (COM1 RS485) with the HMIG3U and not the HMIG5U for the Unitelway protocol?
Issue:
XBTZ9780 cannot be used with the HMIG5U

Product Line:
HMIG3U, HMIG5U, HMIG5U2, HMIG5U21, HMIG5U22

Resolution:
Uni-Telway communication has a stricter requirement about timing sequence that requires a specific hardware time that only the HMIG3U and other non-Windows based Magelis HMIs) possess. Due to the lack of such a hardware timer in the Windows based HMIs, such as the HMIG5U, the Uni-Telway protocol is only able to communicate over RS232 only for this model.

Schneider Electric Global

Attachment(s)
UnitelwayRS485_XBTZ9780cable.jpg [38.51 KB]
Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: