{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to activate DC injection braking [DC INJECTION]- dCI in ATV71 - ATV61 drive?
Hello,

DC injection braking is activated through below parameters

- Stt [Type of stop] = [DC injection] (dCI): DC injection stop ---> when you apply stop command the DC injection braking is active.

- dCI [DC injection assign.] = LI1 to LIx ---> The DC Breaking is activated when you give this assigned Logic input LIx - When you apply this logic input (if assigned) it will apply DC injection breaking.

Please refer the programming manual extract for the related parameter setting.

Schneider Electric Global

Attachment(s)
ATV71-ATV61 DC injection Braking.pdf [108.18 KB]