{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is a BrF fault on an ATV320 drive?
Issue:
BrF fault on an ATV320 drive.

Product Line:
ATV320 drives

Environment:
BrF faults

Cause:
The brake feedback contact does not match the brake logic control. The brake does not stop the motor quickly enough (detected by measuring the speed of the “Pulse input” input.

Resolution:
Check the feedback circuit and the brake logic control circuit.
Check the mechanical state of the brake.
Check the brake linings

Schneider Electric Global